5G NR
The features described in this topic apply to the M9484C VXG only.
Bandwidth part (BWP) is a UE-specific setting, but
Applies to the M9484C only.
Displays the ID of current BWP, it is automatically generated based on the index of the BWP array.
|
GUI Location |
Apps > 5G NR > Waveform > Capability set to Real-time Uplink > Carrier > Uplink > BWP > BWP ID |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:ULINk:BWP:ID? |
|
SCPI Example |
|
|
Preset |
0 |
|
State Saved |
Yes |
|
Initial S/W Revision |
A.10.00 |
Applies to the M9484C only.
Sets the name of the BWP. It is used to select the BWP for the data channel.
|
GUI Location |
Apps > 5G NR > Waveform > Capability set to Real-time Uplink > Carrier > Uplink > BWP > Name |
|
Initial S/W Revision |
A.10.00 |
Applies to the M9484C only.
|
GUI Location |
Apps > 5G NR > Waveform > Capability set to Real-time Uplink > Carrier > Uplink > BWP > Numerology |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:ULINk:BWP:NUMerology? |
|
SCPI Example |
|
|
Preset |
NA |
|
State Saved |
Yes |
|
Initial S/W Revision |
A.10.00 |
Applies to the M9484C only.
Sets the RB offset of the current bandwidth part (BWP) relative to CRB0.
A resource block (RB) consists of 12 contiguous subcarriers. The RB Number determines the contiguous amount of spectrum available to the specified BWP, starting from the RB Offset within the containing component carrier. The maximum number of RBs potentially available to this BWP is determined by the numerology of this BWP and the maximum RB limit specified for the component carrier for that particular numerology.
|
GUI Location |
Apps > 5G NR > Waveform > Capability set to Real-time Uplink > Carrier > Uplink > BWP > RB Offset (N_BWP_start) |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:ULINk:BWP:RB:OFFSet <integer> [:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:ULINk:BWP:RB:OFFSet? |
|
SCPI Example |
|
|
Preset |
0 |
|
State Saved |
Yes |
|
Min |
0 |
|
Max |
274 |
|
Initial S/W Revision |
A.10.00 |
Applies to the M9484C only.
Set the resource block (RB) number of the bandwidth part (BWP).
|
GUI Location |
Apps > 5G NR > Waveform > Capability set to Real-time Uplink > Carrier > Uplink > BWP > RB Number (N_BWP_size) |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:ULINk:BWP:RB:NUMBer <integer> [:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:ULINk:BWP:RB:NUMBer? |
|
SCPI Example |
|
|
Preset |
273 |
|
State Saved |
Yes |
|
Min |
1 |
|
Max |
275 |
|
Initial S/W Revision |
A.10.00 |